2/7/2020 4:56 PM | |
Posts: 174 Rating: (2) |
How to convert ladder logic to STL/SCL in TIA portal 15.1? Cpu s7 1500 |
2/9/2020 12:33 PM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666) |
Hello Jibin.Matthew; Simatic Manager allowed the display of code in various languages (LAS, FBD, STL) and switching the view from one to another. LAD and FBD can be easily converted to STL, STL cacould be conditionally converted to LAD or FBD. The screenshot below is taken form the Programming with Step 7 (Simatic Manager) manual, chapter 9 discusses programming languages. There are also many, many threads on the forum discussing this type of code display conversion: Forum discussion on LAD/FBD/STL display conversion TIA Portal does not allow display conversion, you have to decode your code blocks if you want to use another language. Programming manuals for STL, FBD and LAD for the S7-300/400 families are available on your computer if Simatic Manager is installed, or can be downloaded from the forum (use the search box at the right to locate them). For TIA Portal, the documentation for programming languages is integrated in the system manual if the version of Step 7 you are using: Hope this helps, |
This contribution was helpful to1 thankful Users |
2/9/2020 1:55 PM | |
Posts: 174 Rating: (2) |
Thank you. I know it to switch language in simatic manager. Now I am looking that function in TIA Portal to understand the program. How to decode program in TIA Portal? Can it do manually by looking pdf document or any automatic decoding instruction available in TIA Portal for S7 1500 PLC? I could see the FBD to LAD conversion option in FC properties. Also I can add STL network in FC in TIA Portal. However, how to switch program to other language?? As per your comment, this function (STL to LAD) not available in TIA Portal. I am little bit confused. Please confirm yes or No. I |
Follow us on