2/2/2020 11:24 AM | |
Posts: 7 Rating: (0) |
Hello! I have installed a 802d with Smart Line Module and Motor modules. In the commissioning I think all is fine until I get stuck on STATUS 31 on the Motor modules. STATUS 31 displays the message "Ready to power up - set "ON/OFF1" = "0/1" (p0840)". Can you please help me sort this out? I have not run the Macro 150005 that I think is be ment to setup the X21/X22 without SM? since the Commissioning manual does not describe how to do this. Is this necessary and in that case how do I do that? When I look in STARTER in the motor module control logic p0840 is set by r2090 bit 0. This is not set, is this the correct configuration. In this case what sets the r2090 bit 0? The X21 connection I have at the CU is CU X21.1 - Smart Line module Ready (X21.1) Also I have no EP at the motor modules, not sure if this is correct but I use a line contactor not the "Safety integrated" I'm very thankful for all help! AttachmentArchive.zip (66 Downloads) |
2/2/2020 9:56 PM | |
Joined: 5/24/2016 Last visit: 9/13/2024 Posts: 347 Rating: (52) |
Hello. It does not seem like your OFF signals are correct. How is the wiring from the CU to the Smart Line and Motor module? You say you use a line contactor but have not connected the EP signal? Please see attached files for a connection example and OFF1 and OFF3 example Best Regards Riddersholm AttachmentOFF1 OFF3 EP.zip (92 Downloads) |
2/4/2020 7:19 AM | |
Posts: 7 Rating: (0) |
Hello, I have read that post you linked and it have some tips, but some settings are for Active line module. I will try to run the macro according to this manual page 93. I don't understand why this chapter is removed from the later manuals that I have on the CD that came with the system. I hope this is the correct way to run the macro, but I will use macro 150005 for my machine. Please tell me if this is not the correct way to run the macro for later 802d. Then I will setup the PLC program. Thank you for the help |
2/9/2020 7:49 AM | |
Posts: 7 Rating: (0) |
I setup the PLC program and configured the MD for the axises used in Subroutine 40 (AXES_CTL) and this is setting the drive ready signals. Now it works! |
2/9/2020 7:39 PM | |
Joined: 5/24/2016 Last visit: 9/13/2024 Posts: 347 Rating: (52) |
I am glad to hear that this solved your problem Best Regards Riddersholm |
Follow us on