6/26/2019 1:15 PM | |
Joined: 3/20/2013 Last visit: 1/4/2022 Posts: 4 Rating: (1) |
Hi I am facing the same issue. Webserver V9.0 is running on Windows Server 2016. If I connect from a PC with Win10, everything is working and APL units are displayed. If I connect from a virtuel PC with Windows server 2012, everything is working, except APL units are not displayed. Internet Explorer is version 11 on both Win10 and Win2012 server. Any ideas? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/26/2019 14:43:08New subject after splitting |
|
6/27/2019 8:56 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello munchu, it look like you have missed something by the installation or settings for the Web client. My guess is that you missed something be the web client plug-ins. Do you have installed all web client plug-ins in the right order?
More Information about the web client plug-ins you can find in the manual PCS 7 Web Option for OS in section How to install the plug-ins. With regards |
6/28/2019 2:30 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello munchu, before you install a new Windows server you can look, if the script for the transformation from the integer to text is working. The script is connected to every blockicon under Properties>Links>UnitNumericValue1. You can find a description in the APL Style Guide in section "Links" property group. With regards |
7/1/2019 10:36 AM | |
Joined: 3/20/2013 Last visit: 1/4/2022 Posts: 4 Rating: (1) |
Thank you. I will check the script as well. |
Follow us on