Industry Online Support
Technical Forum
8/21/2013 10:38 AM | |
Joined: 10/31/2006 Last visit: 9/21/2022 Posts: 134 Rating: (33) |
I have a similar problem that when ever I make a change to a page and publish it to web navigator the user loses their online saved configuration and the page goes back to default configured settings. I had to make a work aroundby saving the configuration to an XML file.The user can now save their own settings and load open them as different trends See if the attached page might help you. You may have to change the code to suit yourself and I had to deleted a few itemsoff the page before postingit. Therefore there might be an error if it looks for an item I have deleted, I have not tested it before sending. You also might need to add the following comdlg32.ocx Run this to register it: regsvr32.exe c:\WinCCTRendAddonsInstall\comdlg32.ocx download and install this: msxml6.msi Some of the scripting is different for Windows XP and Windows 7 so remove the portion you do not need PDlL was created with WinCC V7.0 SP3 Update 5 Send me a message if you need help AttachmentSaveTrend.zip (487 Downloads) |
Last edited by: O_Moderator at: 8/22/2013 11:28 AMnew subject after splitting from /tf/WW/en/Posts/76431#top |
|
This contribution was helpful to1 thankful Users |
Follow us on