2/10/2020 1:33 AM | |
Posts: 6 Rating: (0) |
Hi All I trying to build Master Multifunction Push Button for lighting control system. The idea is. first part: - When press the button once, output 1 its go ON or OFF, depends from the previous state - When press the button twice output 2 its go ON or OFF, depends from the previous state - When press the button three times output 3 its go ON or OFF, depends from the previous state after that 2nd part: -When all outputs are OFF and button is press and hold for 2 sec. all outputs will go ON -When one, two or all outputs are ON and Button is press and hold for 2 sec. they all will go OFF. I make some strategy but i'm not happy about this, It's not working smoothly how I want. I delete some strategy to focus on first part. Maybe someone knows how to simplify and make this part better. Any help will be very appreciated. AttachmentCircuit Diagram3.zip (154 Downloads) |
2/10/2020 6:02 AM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32878 Rating: (4064)
|
Here a possible solution from me.
Attachmentpero987_light_control_0BA8.Standard.zip (224 Downloads) |
2/10/2020 7:34 PM | |
Posts: 6 Rating: (0) |
Thanks a lot Ixo65 your are great. That works perfect for me. |
This contribution was helpful to1 thankful Users |
2/10/2020 7:38 PM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32878 Rating: (4064)
|
Hello pero987, you're welcome ... |
This contribution was helpful to1 thankful Users |
Follow us on