2/16/2020 8:00 PM | |
Posts: 1 Rating: (0) |
Greetings, In my system architecture I'm using a S71200 PLC as a gateway between a PROFIBUS network and a Ethernet network. The gateway PLC is collecting information from a PROFIBUS network. The information is then available for another PLC via IEC104 using a master-slave communication. The messages received by the IEC104 master PLC are being received with validity bad. I'm assuming that the gateway PLC is sending the information with validity bad because of the lack of time tag. Can the lack of time tag be a condition to receive validity bad in the master PLC? How can I configure the IEC104 in order to send always the time tag of the gateway and that way solving the validity issue? Thank you in advance, Hugo Oliveira ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/17/2020 07:33:19New subject after splitting |
|
Follow us on