2/14/2020 12:54 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello MarCZ; The CP 1242-7 is a GPRS (wireless messaging) processor. If you want to use it as a "Telecontrol" CP, so you can dowload programs to the CPU, read diagnostics.... you must have a Telecontrol server installed and configured in the CPU. See the following configuration manual for the CP 1242-7: https://support.industry.siemens.com/cs/ww/en/view/109777045 Hope this helps, |
2/19/2020 2:34 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640) |
Hello perhaps this FAQ helps also https://support.industry.siemens.com/cs/ww/en/view/39863979 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on