2/10/2020 5:03 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33798 Rating: (4199)
|
Start the install.htm and follow the instructions. Mac OS X Instructions: Instructions After downloading, double-clickSetup Notes Be sure you have Java installed. You can download Java fromApple's site The compressed installer should be recognized by Stuffit Expander and should automatically be expanded after downloading. If it is not expanded, you can expand it manually usingStuffIt Expander 6.0 or later. If you have any problems launching the installer once it has been expanded, make sure that the compressed installer was expanded using Stuffit Expander. If you continue to have problems, please contact technical Support. -------------------------------------------------------------------------------------------------------------------------- Please note: LOGO!Soft Comfort doesn't Support all MAC versions. Suggested operating systems LOGO!Soft Comfort V8.2.1 supports the following operating systems: ●Windows: Windows XP, Windows 7, Windows 8 or Windows 10 with the following requirements: – PC with Pentium IV processor – 500 MB free hard disk space – 512 MB RAM – SVGA graphics card with minimum of 800 x 600 resolution (at least 256 colors) – DVD-ROM ●Mac OSx: Mac OS X 10.7 Lion; Mac OS X 10.8 Mountain Lion; Mac OS X 10.9 Mavericks; Mac OS X 10.10 Yosemite; Mac OS X 10.11 X El Capitan. ●Linux: Tested with SUSE Linux 11.3 sp3, kernel 3.0.76. Compatible with all Linux distributions which are aligned with Java 2. You can find the necessary hardware requirements from the corresponding Linux distribution. ●Java Runtime Environment 1.8.0_121, which is recommended Version. -------------------------------------------------------------------------------------------------------------------------------- In your case I would start a Support Request. AttachmentLOGO!Soft Comfort V8.2.1 (InstallAnywhere Web Installer).pdf (186 Downloads) |
Last edited by: ixo65 at: 02/10/2020 05:05:24 |
|
This contribution was helpful to1 thankful Users |
Follow us on