2/23/2020 9:40 PM | |
Joined: 7/6/2009 Last visit: 6/1/2022 Posts: 100 Rating: (0) |
Hello , I am using SINEMA RC Server running on VM Ware virtual machine , I have configured two users and started to configure devices Started with first one SCALANCE M876-4 which has the attached configurations at SINEMA RC server Side and at the modem itself Modem is connected to internet and working properly and connecting to the Sinema RC server , getting the details of configuration ( device name ) correctly. However, it's not establishing VPN Tunnel at all , it's always giving the status shown in attached picture. I have reviewed the password , certificates , everything is fine . even tried many times to delete the device and configure it from zero .. even changing modem itself ....No chance In the same time , both of users are working properly . Communication with server , logon , establishing VPN tunnels all are working fine in fact , i can't find or guess where may be the problem preventing establishing VPN between serer & modem appreciate if anyone can guide
AttachmentSCALANCE M876-4 SINEMA RC Configuration.jpg.pdf (136 Downloads) |
Walid Elshazly |
|
Follow us on