2/24/2020 8:38 AM | |
Posts: 17 Rating: (0) |
Hi, Currently I have sensor which is only capable to send RS-485 signals. The PLC I'm using now is CPU 314C-2-PN/DP with a CP341 RS-422/485 module. Now, I would like to change the configuration to all sensors' signal to tie in directly to PLC individually. Hence, I've used a converter to convert MODBUS RTU to MODBUS TCPIP. Each sensors will have their specific IP Address. Will I be able to configure the PLC to read MODBUS TCPIP via SCALANCE X116/X108 or in fact any SCALANCE product? ------------------------------------------------------------------------------------------ AttachmentSystem Achitecture.pdf (70 Downloads) |
Last edited by: Jen_Moderator at: 02/25/2020 06:23:56New subject after splitting |
|
Follow us on