2/25/2020 10:55 AM | |
Posts: 3 Rating: (0) |
J'ai le même problème avec tp177b et s7-1200. s'il vous plaît comment puis-je trouver tp177b dans tia V15.1? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/25/2020 12:51:37New subject after splitting |
|
2/25/2020 11:09 AM | |
Joined: 12/18/2014 Last visit: 5/7/2024 Posts: 32983 Rating: (4076) |
TIA V15.1 doesn't support the TP177B. |
2/25/2020 2:17 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
TP177B can be configured as from WinCC flexible 2005 compact version or higher Please see the panel description and technical data: https://support.industry.siemens.com/cs/ww/en/ps/6AV6642-0BC01-1AX1 The current version is WinCC flexible 2008 SP5 Compact It's part number: 6AV6611-0AA51-3CA5 Hope this helps.
|
Ayman Elotaify |
|
2/25/2020 3:05 PM | |
Joined: 4/12/2018 Last visit: 5/1/2024 Posts: 24 Rating: (0) |
The latest TIA version that supports the TP117B is version V14, so you can migrate to TIA V14 if you want. If needed, you can split the project in PLC (V15.1 / V16) and HMI (V14), the downside of this is that you have to maintain the tags in both projects, because they're not linked anymore (device proxy doesn't work from old to newer version). See also PLC in TIA v15.1 and HMI in TIA v14
|
Valar morghulis / Valar dohaeris |
|
2/26/2022 11:29 AM | |
Joined: 7/22/2019 Last visit: 3/23/2024 Posts: 7 Rating: (0) |
It is a shame that the widely spread OP/TP177B panels were omited from TIA portal V15 upwards. |
Follow us on