2/27/2020 6:56 AM | |
Joined: 6/12/2014 Last visit: 4/26/2024 Posts: 59 Rating: (0) |
Hello There, I am trying to configure redundant IOs in redundant 400 station.I am able to do this over profibus IM153 where as over profinet IM153 ,I am not able to select the redundant module.The tab to this setting is missing.Please have a look at the attached backup and suggest the right settings. Thanks in Advance Parmod Takkar AttachmentTest_red.zip (28 Downloads) |
2/19/2021 5:37 PM | |
Joined: 5/27/2019 Last visit: 3/1/2024 Posts: 1 Rating: (0) |
I have the same problem as you. Have you then solved? |
2/19/2021 8:52 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello Peewy (and Ptakar, sorry for the late reply); Profinet works differently than Profibus because of he physics that it uses as support. Redundancy with Profinet operates on basis of MRP, and redundant rings basically, and 2 redundant I/O modules will be controlled by both masters simultaneously over Profinet, whereas with Profibus they would be controlled alternatively by one or the other master. To make things clear, you should study the following document: - Configuration examples for S7-400H over Profinet as of v6.0 https://support.industry.siemens.com/cs/ww/en/view/90885106 Hope this helps, |
Follow us on