3/2/2020 7:41 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello KumarPra, if there is no automatic switchover of the Client, https://support.industry.siemens.com/cs/ww/en/view/109763043 For a manually switch over you can only stop the runtime
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
4/8/2022 1:29 PM | |
Joined: 1/14/2020 Last visit: 9/11/2024 Posts: 13 Rating: (0) |
Hello Georg, Is it possible to manually force switch-over between redundant servers, i.e. switch Active server to Standby and Standby to Active without stopping Runtime? Regards, Vytenis |
4/11/2022 2:29 PM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13728 Rating: (1728) |
Hello vytenisg Yes you should be able to switch by using the @RM_MASTER tag. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on