7/9/2018 3:53 PM | |
Joined: 3/31/2009 Last visit: 7/16/2024 Posts: 191 Rating: (3) |
Dear Expert, i like to access wincc alarm dan tag logging from vb.net, as per manual that i read, i have to used WinCCOleDBProvider. according from previous post on this forum, i read if i install wincc, winccoledbprovider driver are automatically installed on the windows system. From the OLEDB provider driver on windows i cannot found winccoledbprovider, how do i get the winccoledbprovider driver ? OS : Windows 7 Pro 64bit Installed software : WinCC RC v7.4 WinCC Connectivity Pack Server BR Rusli Attachmentpicture.zip (177 Downloads) |
7/9/2018 11:36 PM | |
Joined: 9/19/2009 Last visit: 9/21/2024 Posts: 459 Rating: (85) |
Hi Please, see the picture attached and you will find the driver. If I´m not wrong, You have create a file *.udl and you don´t see but you have it. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
3/2/2020 1:11 PM | |
Joined: 2/25/2016 Last visit: 9/19/2024 Posts: 2 Rating: (0) |
Hi Rusli I am also getting the same issues. Did you ever resolve your problem? |
Follow us on