3/6/2020 9:22 AM | |
Joined: 1/21/2016 Last visit: 3/6/2024 Posts: 87 Rating: (11) |
Hello, I have a mechanic with 2 motors controlled by 2 S210. I have a translation movement to perform. The two motors are synchronized. The problem is that I can not do the tunning of only one engine at a time, the mechanics do not allow me, indeed the two axes of translation are mechanically linked (I attached a diagram to understand (Sorry I'm not very good at drawing). I would like to know if it was possible to perform an auto tuning in synchronization. Cordially. AttachmentSchéma.pdf (79 Downloads) |
Cordially, |
|
3/6/2020 11:36 AM | |
Joined: 4/28/2015 Last visit: 10/20/2023 Posts: 43 Rating: (6) |
-Removed- |
Last edited by: Axel Scholz at: 03/06/2020 17:10:18Grüße, Axel |
|
Follow us on