3/5/2020 12:54 PM | |
Joined: 11/27/2018 Last visit: 9/18/2024 Posts: 12 Rating: (0) |
Hello Georg, SIMATIC NET V16 installed as well. I think that the problem is resolved with the latest update. I saw your post about update 2 this morning, so downloaded and installed it. Yet still wondering why this happened with some tags and not with all of them. Also curious what to do with other installations from custumers. I attached the log file. Thank you in advance. AttachmentSIMATIC_S7_PROTOCOL_SUITE_01_LOG.txt (205 Downloads) |
This contribution was helpful to1 thankful Users |
3/10/2020 8:18 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello LD5804, then should you use the SIMATIC Assessment Suite - Data Collector (SAS-DC) - https://support.industry.siemens.com/cs/ww/en/view/65976201
Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on