3/4/2020 10:50 AM | |
Joined: 4/20/2017 Last visit: 10/5/2023 Posts: 21 Rating: (0) |
Hello WinCC community, I have got problems with the project C-script after updating WinCC from 7.2 to 7.5. The script retrieves a list of WinCC-users from the SQL-database and populates the fields of the ComboBox element. But after that update, it ain't work: the ComboBox has got empty list. I still can’t understand what the problem is. I've attached C-script in txt-format. My abilities are not enough and I turn to a reputable community for help.
AttachmentLogin.txt (69 Downloads) |
Last edited by: Automateur at: 03/04/2020 13:49:53 |
|
3/5/2020 6:34 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (81) |
Hi Automateur The most easy solution is not use the ActiveX and use the native combobox of WinCC. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
6/5/2020 10:13 AM | |
Joined: 10/16/2016 Last visit: 5/3/2024 Posts: 4 Rating: (0) |
Hi! Do you find any solution? Combo Box native does´t works thanks |
Follow us on