3/2/2006 8:12 PM | |
Joined: 9/23/2005 Last visit: 9/19/2024 Posts: 4347 Rating: (1446) |
Hi, it's necessary to have more dectails to be precise in a answer, but some considerations: is it dips of the OLM right configured? Is the profibus parameter adjusted for a ring operation? See FAQ: http://support.automation.siemens.com/WW/view/en/1995199 and also the FAQs: http://support.automation.siemens.com/WW/view/en/22561265 http://support.automation.siemens.com/WW/view/en/22345036 http://support.automation.siemens.com/WW/view/en/19758281 |
Denilson Pegaia |
|
3/3/2006 2:36 AM | |
Joined: 3/2/2006 Last visit: 7/15/2008 Posts: 29 Rating: (2) |
Hi, Mr Pegaia In fact, we are not using OLM's. We are using some PTD relays that already have double fiber optical ring connection. And, as you can see on the attached file, there are not so many options on the Profibus DP configuration... Thanks, Paulo Zerbati PS: E ai, Denilson! Tudo bem? Eu sou o Paulo, que trabalhava na PTD EA. Agora estou trabalhando aqui na China. Qualquer coisa que voces precisarem por aqui, e so dar um toque. Meu e-mail e paulo.zerbati@siemens.com. Abraco, Paulo Attachment7UT612 PROFIBUS.zip (745 Downloads) |
4/26/2006 5:48 AM | |
Posts: 26 Rating: (2) |
Hi, |
Follow us on