3/11/2020 9:19 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735)
|
Hello The WinCC V7.3 Project you have to migrate first to WinCC V7.4 Sp1-> then you can migrate to TIA Portal V15.1 WinCC Professional. I would do this in a seperate Step. for the migration of WinCC Flexible 2008 Sp5 an the Simatic Manager Project you need an installation of both (classic and TIA) on the same system or you use the TIA Migration Tool then you can do the migration in two steps on the different Systems. Here are general Information to this Topic: https://support.industry.siemens.com/cs/ww/en/view/83558085 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on