3/12/2020 10:37 AM | |
Joined: 9/20/2018 Last visit: 1/2/2024 Posts: 42 Rating: (4) |
Hello Everyone, I am also Facing one issue. I am using 6ES7331-7TF00-0AB0 along with IM 153-4 which is on PROFINET. Sometimes transmitter which are connected in Channel of card is showing in WINCC though Value is Correct. If I check Diagnostic then it is showing ADC/DAC error ( Internal Fault). After unplugging and plugging Card from rack all red wrench are disappearing.Again it will come after 2-3 days. I am having around 6 IM 153-4 on PROFINET all IM having only AI card NO DI and DO . If any 1 card showing error then it is showing in all other card also. In result All the instrument in Plant showing red wrench. To resolve this issue again I have to unplug all AI card and Plug it again. In my Case module is configured for 2 Wire. Still I have connected 1- 4 wire Instrument to Module. All the wiring is done correctly as shown in manual. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/12/2020 13:30:37New subject after splitting Last edited by: AutoGen_6024931 at: 03/13/2020 04:24:20 |
|
Follow us on