3/10/2020 5:13 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
Maybe the original file will help you, see attachment. There is also an excel sheet and you can type in any bit, byte or word on the right side (see column M/N). But first select the start address in J1 (0 or 1) to get the right values for the complete table. The start address depends on the Modbus partner. Regards, Scorp AttachmentModbus Tabelle.zip (272 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on