3/17/2020 1:15 PM | |
Posts: 19 Rating: (0) |
Morning all, i'm having a bit of a head scratch here i have attached a program that i have uploaded and i have noticed a few odd things and the first is that in transition from my pc to the logo the program gets altered and i have no idea why i have factory reset the Logo prior to the upload. also the temperature is stuck at -50c i have replaced the AM2 with a AM2 RTD and a new PT1000 sensor. All help is greatly appreciated Thanks in Advance Neil AttachmentUploaded.zip (80 Downloads) |
3/17/2020 1:17 PM | |
Posts: 19 Rating: (0) |
attached is the program that i downloaded from the Logo after i Uploaded the original program Thanks in Advance Neil Attachmentdownloaded.zip (58 Downloads) |
3/17/2020 3:11 PM | |
Posts: 19 Rating: (0) |
Here is what i downloaded from the LOGO and as you can see it has changed to configuration of the switches.? |
Follow us on