9/25/2017 3:32 PM | |
Posts: 52 Rating: (1) |
Hello Friends, I am facing problem For alarm Logging. I am generating alarm through VBS Scripting.Following are my code. Function WinCC_Message1(Byval TagName, Byval TextMessage) HMIRuntime.Tags(TagName).write 1 HMIRuntime.Tags(TagName & "_text").write TextMessage HMIRuntime.Tags(TagName).write 0 End Function For this i am Using Alarm bit=1 (binary bit ) and Alarm text = (16 bit text tag). Button Script for alarm activation. Call WinCC_Message("wincctestalarm1", "This is wincc alarm 2 with timestamp: " ) Problem facing for this is when i trigger alarm Alarm get activated in alarm logging but in that Alarm text (text will not show frist time). When i activate alarm on second time then i can see the alarm text. Is any one know how to resolve this alarm functionality. I have attached screenshot for my alarm configuration. Thnak you in Advance. Amol AttachmentScreenShots.zip (248 Downloads) |
This contribution was helpful to1 thankful Users |
9/26/2017 11:18 AM | |
Posts: 52 Rating: (1) |
Thank you for Feedback, it very help full. Just i have one question how i can reset that bit ( HMIRuntime.Alarms(1) ). Thnak you Amol |
9/26/2017 5:04 PM | |
Posts: 52 Rating: (1) |
Hello Georg Berghof , My Problem Solve, i did some setting in alarm logging . Thank you For Help Georg |
3/18/2020 10:36 PM | |
Joined: 11/30/2017 Last visit: 11/8/2023 Posts: 6 Rating: (0) |
Hallo, wich setting you do on the alarm logging to reset the alarms. |
Follow us on