3/20/2020 12:49 AM | |
Joined: 4/28/2015 Last visit: 4/19/2024 Posts: 4 Rating: (0) |
Hi, I'm having the exact same problem, over Windows 10 1806. I have a project developed in WinCC v7.5 Update 3, that works perfectly fine, after I installed the SP1 (without any update) I'm facing the topic's problem, specially with picture windows with tag prefix (my own faceplates), some tags are read others not... What I did was to rollback the intallation to v7.5 Update 3... I was thinking of installing the Update 2 of SP1 but collegue said it did not work either. Is there any solution for this problem? I'm developing a project right now that needs to use Windows Server 2019, and the only version tested for this operational system is the 7.5 SP1 and its updates... What should I do now? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/20/2020 05:50:59New subject after splitting |
|
4/19/2021 11:43 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello Devendra Patel, you have installed WinCC V7.5 SP1 without any update. You should install the actual Update for WinCC V7.5 SP1. https://support.industry.siemens.com/cs/de/en/view/109773812
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on