3/22/2020 11:02 AM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating: (9) |
Dear All, I have a system of CPU 1512SP-1PN (192.168.0.1) connected with 3 sets of IM155-6PN ST with IO modules (192.168.0.2, 192.168.0.3, 192.168.0.4). 1. TIA Portal "sees" all three IM155 as available devices" (pls see a picture attached) 2. But the PLC can connect via Profinet only to 192.168.0.4 and the others are unavailable via Profinet (pls see a picture attached ) All three baskets of IM155 have the same set of IO modules. Cable length between the stations is 5m (developing in the lab). TIA Portal v15 upd 4. Could you please give an advice where the problem can be Thank you! Attachment1.zip (179 Downloads) |
3/22/2020 3:47 PM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating: (9) |
Dear Hati, your advise has helped, thank you. |
3/22/2020 4:44 PM | |
Joined: 9/21/2012 Last visit: 9/23/2024 Posts: 4161 Rating: (464) |
Would you care to share what the problem was? |
Follow us on