3/21/2020 6:26 PM | |
Posts: 49 Rating: (1) |
Hello friend, i am using TIA protal V16 (STEP 7 & WINCC PROFESSIONAL V16) i have also same problem. when i deactivate (stop the runtime) the runtime, runtime not deactivating 100%. its stop on global script runtime 40% and further process not completed. i am tray apadig but in output window no any text show. my project script , project and other file as per below. please hepl me. - WinCC_Sys_01 - PMDeactivate - PMDiagnose thanks in advances ------------------------------------------------------------------------------------------ AttachmentNew folder (3).zip (34 Downloads) |
Last edited by: RRAAHHUULL at: 03/21/2020 18:45:43Last edited by: Jen_Moderator at: 03/23/2020 11:42:29New subject after splitting |
|
3/23/2020 11:42 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Wincc prof RT V16 not deactivating 100% is published within the conference SIMATIC WinCC (TIA Portal). Best regards |
Follow us on