3/22/2020 11:18 AM | |
Joined: 4/8/2009 Last visit: 9/23/2024 Posts: 83 Rating: (1) |
Dear sir/Madam, We have WINCC server and five client stations system(WINCC 7.0 SP2). System was running fine since 3-4 years. Currently master WINCC server is running fine but standby WINCC server is not going in runtime mode and showing below pop up messages during runtime activation process. 1. "Logging in database on computer dfscada1 is currently inactive." 2. "The use time of your software license has expired! Please obtain valid license." Please find attached screen shots for above pop up messages detail. I found that while opening automation license manager, the same above massage No.1 is showing. In automation license manager, 3 licenses are showing "License is corrupt" massage. Please find attached screen shots for license corrupt massages. Please help me to resolve this issue. Installation of licenses (for corrupt licenses) will solve the issue.? Thanks in advance.
AttachmentLicense pop up.zip (41 Downloads) |
3/23/2020 11:15 AM | |
Joined: 4/8/2009 Last visit: 9/23/2024 Posts: 83 Rating: (1) |
Thank you for your support.. i will raise support request. Regards Sacheen |
3/24/2020 6:35 AM | |
Joined: 4/8/2009 Last visit: 9/23/2024 Posts: 83 Rating: (1) |
Dear sir, License problem is resolved. but WINCC runtime is stop/stuck during activation process of "initializing archive management". when i disable/unchecked alarm logging and tag logging in startup option then only winnc runtime activating successfully. i created another test project but same issue is coming. additionally when i open automation license manger following message is appearing. "Logging in database on the computer dfscada1 is currently inactive." Please find attached screen shots and ALM Emergency log file (.CSV File) in for your reference. Please help me to resolve this issue. as system is running only with one server. Thank you in advnace AttachmentWINCC ALM error.zip (38 Downloads) |
Follow us on