11/22/2019 2:43 PM | |
Joined: 7/24/2016 Last visit: 12/6/2023 Posts: 14 Rating: (0) |
Hi , I am Using MM 440 5.5 kw VFD for a Conveyor application as an Open loop Control.Recently i have faced a Breakdown that after Drive On Command ,Drive Status is "Run" and Have actual speed status also ok and matching with "Set Speed" .But Due to Motor Terminal were removed at drive ,Physically there no motor Run . Hence i wish to Triggered a Fault in drive for the above kind of Scenario ,So that for No motor Cable connect and i have a ready start command ,Drive should stop with a fault . can someone help me on this topic . Advance Thanks. Santosh ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/25/2019 09:28:20New subject after splitting |
|
3/27/2020 12:52 PM | |
Joined: 7/24/2016 Last visit: 12/6/2023 Posts: 14 Rating: (0) |
Thanks dear for your support ..it helped me . |
This contribution was helpful to1 thankful Users |
Follow us on