3/25/2020 9:18 PM | |
Posts: 3 Rating: (0) |
Hi I am trying to use PUT instruction, i am not getting any error while doing so but the done bit is not healthy as well. Attached is the picture Thanks Vijay ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/26/2020 10:33:02New subject after splitting |
|
3/26/2020 11:00 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585)
|
Hi, it´s not allowed to use a clock at the Request. PUT/GET are instructions who run for more than one PLC cycle. Use done or error to start request again. Also check (safe) status if error gets 1 How do you evaluate the status of system blocks in STEP 7 (TIA Portal)?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
3/27/2020 9:59 PM | |
Posts: 3 Rating: (0) |
Hi All, I was able to get the same working and attached is the picture for reference. 1) I deleted the connections and made once again 2) Also changed the BYTE to INT
|
Follow us on