3/29/2020 3:27 PM | |
Posts: 2 Rating: (0) |
Can i somehow configure the VPN correctly if remote PC has only one NIC interface? I wasn't able to fully configure TeamViewer VPN on remote PC where there were 2 NICs, one for internet and one for PLCs. I was able to ping remote PC on both IPs, external TV IP and internal IP after i added that IP with route command and registry edit. But that's all, local PC still wasn't able to ping or connect to any PLCs. So i disabled second NIC, the one internet was connected, and give access whole inner network to internet. Internet has no public IP so the only way to access is by TV now. But with this solution i can't even ping remote PC with inner IP, even with route add command. I wonder why. I have TV with VPN enabled, i can connect to remote PC both to desktop or to VPN using TV IP, i have set IpEnableRouter (confirmed with ipconfig command) and set proper route rule. Remote PC has inner IP 192.168.70.195, and 192.168.70.200 for second NIC which is disabled now. Was able to ping both IPs before when internet was on *.200. Before when i had internet on *.200 IP then *.195 had no gateway setting. Now to give access to internet i had to set gateway to the IP of the device which give internet access. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/30/2020 11:43:28New subject after splitting |
|
Follow us on