3/27/2020 9:23 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, With the help of OS permissions, you can customize the MotSpdCL block according to your needs. For example: OS_Perm bit 6: 1=Operator can start the motor in reverse. -> Set the value to 0. In this case the "Reverse" command is greyed out. |
Last edited by: Oreca at: 03/27/2020 09:24:25If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/28/2020 3:25 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
If your plant doesn't have reverse vfd control, feel free to modify the faceplate @PG_ file. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/31/2020 2:19 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear DDo84, Yes, connect SP_Out to Rbk. But....Please do a small logic. by using Sel_R block, when Fbk Run (From field) =1, SP_Out = Rbk, if FbkRun=0, Rbk=0. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on