3/31/2020 5:57 PM | |
Posts: 46 Rating: (0) |
Hi, It seems to work now, in on line simulation mode the M1 one is flashing, but sometimes it stops very short, is that normal ? The pump is working with a continue flow I need a program to show the actual flow in m3 per hour or l/sec or minutes, someone idees ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/01/2020 06:48:30New subject after splitting |
|
4/1/2020 6:52 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7966 Rating: (162) |
Closed cause question posted twice. The second thread with the subject Need the water flow in l/sec or l/min knowing that the tube internal diamer is 42mm is published within the conference LOGO! - Projects. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on