3/31/2020 2:36 PM | |
Posts: 25 Rating: (1) |
Hi All. I have some problems with an periodic error in our machine. The error comes one or two times in day. Error Number Error 20005 : Device type:1, log. address:322 faulted. (Bit:0, encoder number:0, reason: 0x4h It means drive disconnected itself. i have checked there is no alarm in sinamics integrated . Here with i have attached device log file Can anyone help us to solve the issue AttachmentDevice Diagnostics 31032020.txt (249 Downloads) |
Last edited by: BasicLearner at: 04/01/2020 05:19:43 |
|
Follow us on