4/1/2020 9:17 AM | |
Posts: 50 Rating: (0) |
Dear experts, How create fc,fb in blocks by using source floder. Please explain once. Thanks you |
4/1/2020 12:35 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684)
|
Hello RmnChowdary; What is not working? What is the name if the source file you want to compile? How was it generated? Please show a screenshot of the contents of the Blocks/Source folder. You can generate a source from Step 7. There is z complete chapter on the subject in the Programming with Step 7 v5.5 manual (ch. 13, Crrating STL source files): https://support.industry.siemens.com/cs/ww/en/view/45531107 You can open the source file in Word or Notepad, modify it, add DBs or other blocks to it, change its name, save it in the Source folder and compile it again. We used source files to send a number of blocks we were programming to another user, by email for example, so he could compile them, open the compiled blocks in Step 7, verify and correct them if need be. And then send them back for incorporation in the final program. Hope this helps, |
Last edited by: dchartier at: 04/01/2020 12:38:39 |
|
This contribution was helpful to1 thankful Users |
Follow us on