10/3/2019 2:55 PM | |
Posts: 1 Rating: (0) |
Hi all, Just a quick question about the XML produced when exporting by the Siemens OPC UA Modelling Editor (SioME). I am having some XML parsing errors when I try to import the file as part of a server configuration. I am trying to debug whether the problem is with the XML file, the OPC UA SDK I'm using for the server, (or most likely the case - myself). In this example: from SiOME I create a simple Structured Data Type (TestStructure) with a single Structure Item (TestItem, a Boolean). A snippet is below, and the full XML is attached.
When I add the inverse 'HasEncoding' references manually to the XML file after exporting from SiOME (the lines directly beneath the comments above), the server is able to import the XML file. Creating the same example using a different modelling tool (UAModeller), it adds these inverse references automatically and there is no problem importing the resultant XML file. The OPC UA Specification (Part 3 - Address Space 1.04, 5.8.4) specifies (emphasis mine) that:
Does this imply that these inverse 'HasEncoding' references should be present in any case in the XML generated by SiOME? Thanks, Harry Attachmenttest_structure_bool.txt (116 Downloads) |
This contribution was helpful to1 thankful Users |
4/2/2020 1:52 PM | |
Posts: 1 Rating: (0) |
I ran in exactly the same problem as described by harryking almost 1 year ago. How has this mandatory extension not been integrated into SiOME yet? |
Follow us on