4/2/2020 2:18 PM | |
Joined: 1/24/2015 Last visit: 10/27/2021 Posts: 193 Rating: (7) |
Dear All Experts; I want to wish everybody healthy days. I am trying to make a program by using ramp function. But I should add a feature to this function. I will use it for calculating setpoint. But in my program I will add a hold situation. Also the operator can be hold the set number as a desired value. as of right now everything is ok. But when it is in hold position I want to set the calculated automatic value. Even I activate hold situation, it is going on calculating at background but I cannot this value. I want to see it even I activate hold position. I attached the program, I simply used program control operation jump function.
Best regards. AttachmentRamp_function.pdf (39 Downloads) |
Last edited by: Mert Turgut at: 04/02/2020 14:19:05 |
|
Follow us on