4/1/2020 8:31 PM | |
Joined: 8/23/2019 Last visit: 8/29/2024 Posts: 58 Rating: (0) |
Hello every one, so many time I tried to Migrate Project Tia Portal V15 to V14 or V13 but doesn't work. I used Migration Tools Tia Portal from siemens, https://support.industry.siemens.com/cs/ww/en/view/58638200 I just have TIA PORTAL V14 and V13 It doesn't worked. so please help me to any one can migrated this file to V14 Tia Portal. I do appreciated thank you very much SS |
Last edited by: Solusi Industri at: 04/02/2020 01:41:50Last edited by: Jen_Moderator at: 04/02/2020 08:30:40Optimized link. |
|
4/1/2020 8:49 PM | |
Joined: 9/21/2012 Last visit: 9/20/2024 Posts: 4149 Rating: (464) |
It's not possible to migrate to a lover version of TIA Portal. You need to re-write the code to earlier versions. |
4/2/2020 6:50 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
The migration tool associated with TIA Portal is for migrating S7-300/400 projects from class Step7 to TIA Portal. Has nothing to do with versions of TIA Portal. Hope that clears up what the tool is there for. If you have SCL blocks, you can export them easily by Generating blocks from source, saving as an .scl file. Then import external source files and add all the .scl files, and generate blocks from source. You can export tags to a .csv file and import into another version of TIA Portal. If you use TIA Openness, you may be able export some other parts of the project, but will likely be a problem without software efforts. For most projects, it's quicker to use 2 monitors and have both versions open and transfer them between versions that way.
|
science guy |
|
Follow us on