4/13/2020 8:30 AM | |
Joined: 11/16/2018 Last visit: 7/6/2024 Posts: 6 Rating: (0) |
Hi Experts, I have a S7 315 2dp cpu with FM352 CAM module on same rack. Every time I switch it off then on the cpu initializes then goes to stop mode as soon as the FM module run LED flickers. The only way the CPU goes to RUN MODE is ; If i delay the booting of the FM module by unplugging the 24V power. I have programmed the an output(to power the FM module) to be set in OB100 to overcome this problem. How else do i fix this problem... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/14/2020 11:25:39New subject after splitting |
|
Follow us on