4/9/2020 4:33 AM | |
Posts: 19 Rating: (0) |
Hi! I am completely new in the LOGO environment! I am working on my dissertation and I need the Temperature and Humidity results from a CR6 DataLogger of Campbell Scientific (https://s.campbellsci.com/documents/us/manuals/cr6.pdf). I am currently working in how to extract the information from the CR6. But I need your help on the LOGO programming, I have seen a lot of posts in the forum and I want to ask for your help. How do I map these entries, like how do I put them on LogoComfort, I have seen a lot of videos of master/slave applications between LOGOs but I cant find one connecting and external device as an slave. The temperature and humidity readings are needed to do an automatization control system, Thank You!! |
4/9/2020 4:39 AM | |
Joined: 12/18/2014 Last visit: 5/12/2024 Posts: 33020 Rating: (4079)
|
Why do you make a new topic for the same problem? You have a own topic: |
4/9/2020 10:01 AM | |
Joined: 2/22/2008 Last visit: 5/10/2024 Posts: 2698 Rating: (206) |
See attachment for Logo as master = Modbus client with some comments in the example program. Regards, Scorp AttachmentModbus-Client.zip (206 Downloads) |
This contribution was helpful to2 thankful Users |
4/9/2020 9:35 PM | |
Posts: 19 Rating: (0) |
Hi Scorp! Thanks for the answer, but the program doesn't open, it shows an error. I have LogoSoft 8.0 |
4/9/2020 9:44 PM | |
Joined: 12/18/2014 Last visit: 5/12/2024 Posts: 33020 Rating: (4079)
|
If you want to work with Modbus and a 08-0BA0 LOGO! you need a newer LSC Version. If you have a full version of LSC V8.0 (not a demo), then can you upload for free the upgrade to the actual version V8.2.1. You can download it here: LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) It's a 1,3 GB sized complete package. Start the install as a administrator. When install is complete then can you open the file from user Scorp. |
This contribution was helpful to1 thankful Users |
4/9/2020 9:55 PM | |
Posts: 19 Rating: (0) |
perfect! Will do that and then come back! |
This contribution was helpful to1 thankful Users |
4/10/2020 12:32 AM | |
Posts: 19 Rating: (0) |
This is perfect! The comments really help me out! [snip] |
Last edited by: Jen_Moderator at: 04/14/2020 06:49:03Division of questions into separate topics. |
|
Follow us on