4/13/2020 8:10 PM | |
Joined: 12/16/2015 Last visit: 12/27/2023 Posts: 5 Rating: (0) |
Hello experts, I hope you can help me clarify the migration process in this case. I have the project originally from V7.1 SP4 that is using blocks from older library version. But while analising the versions of function used in each AS, I realized that some of the functions belonging to PCS7 Library are from an older version then expected instead of PCS7 Library V7.1 SP3. For example: AS3 uses FB61 CTRL_PID v1.11 but Library V7.1 SP3 has V6.0 Can I leave this function in V1.11 while migrating to PCS7 V8.1 SP1? I know that I have to replace channel blocks. But what do I have to do with the other blocks like CTRL_PID, MOTOR etc. What are the consequences/problems of not replacing them? According to Kompatibility tool, to migrate to V8.1 SP1 I would need to install aditional older libraries: - library V7.1 SP3 Upd4 - basis library V7.1 SP3 Upd11 - faceplates v7.1 sp3 Upd1 - APL not in use I looked in every AS for functions belonging to a library that are in use. I used an excel file (attached) with the list of functions/versions from (library and basis library v7.1 sp3 updx in different sheets) and checked if that version was in use in the project (yellow mark different versions)!! So from this analisis I get some yellow marks were I need to upgrade functions from older versions. But do I really need to do it for every block? Thanks in advance AttachmentPCS7 MIGRATION - libraries analisys.xlsx (87 Downloads) |
Follow us on