4/17/2020 2:12 PM | |
Joined: 1/14/2009 Last visit: 4/24/2024 Posts: 19 Rating: (0) |
Hi guys, Got a trouble please help. Client: CPU1513(1AL01) V2.8.1 Server: CPU1212C V4.4 OPC security policy: Basic256SHA256, User authentication reqired. The server works with UaExpert, not with CPU1513, FB OPC_UA_Connect error code:0x8013 0000, meaning: BadSecurityChecksFailed 0x80130000 An error occurred verifying security. They only works if change security policy to None and Anonymous login. 2 CPU configured in diff. project. Client accept server certificate automatically, client certificate ported to the server. Any idea? BR, Corben Attachments7-1xxx ua isue.zip (157 Downloads) |
Last edited by: Corben at: 04/17/2020 14:18:38 |
|
4/17/2020 4:31 PM | |
Joined: 1/14/2009 Last visit: 4/24/2024 Posts: 19 Rating: (0) |
Now I copied the 2 CPU into one new project, renew certificate and settings for both, guest login, error status code is: BadCertificateInvalid 0x80120000 The certificate provided as a parameter is not valid. Corben Attachments7-1xxx ua isue2.zip (158 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on