4/16/2020 11:09 PM | |
Joined: 2/8/2018 Last visit: 7/21/2024 Posts: 61 Rating: (2) |
Hello dchartier Here some screen shots But regarding L data - Physical addresses are lokal data as well? AttachmentScreenShots.zip (76 Downloads) |
4/18/2020 12:36 AM | |
Joined: 2/8/2018 Last visit: 7/21/2024 Posts: 61 Rating: (2) |
Hello jacek d I've got access to the code in fb1610 and I can see that your second explanation is the answer. You can see the code yourself and maybe I miss something . But what I can see it does not care of area identifier. Regardig Local data: I wrote Physical addresses because I saw that somewhere here on the forum, but what I understand about L-data is , if for example we have some FB which is called from say OB1 the local data of FB are Temp var only. Correctt me if I am not right Thanks AttachmentFB1610.pdf (88 Downloads) |
Follow us on