4/28/2020 5:26 AM | |
Posts: 1 Rating: (0) |
Hi, I have S7 1515-2 PN PLC - X1 interface is assignd with IP 192.168.0.1 and is connected to TIA (v14.1) Machine - X2 interface is configured as i-device and IP-address assigned is 10.1.26.55 (255.255.255.0) - When compiled and loaded configuration, no error seen - But there is diagnosis CPU maintenance demanded: Emergency IP suite parameter for IE interface activated temporarily assigned new IP address 10.1.26.55 PLC_1 / Current CPU operating mode: STOP - On scanning with PRONETA i found it sets gateway as 10.1.26.55. - It fails to connect with another profinet controller... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/28/2020 12:10:45New subject after splitting |
|
Follow us on