4/26/2020 10:44 PM | |
Joined: 6/20/2013 Last visit: 3/14/2023 Posts: 1 Rating: (0) |
Hi everyone! I have a project made with TIA Portal v15 upd 4 (it includes HMI, PLC, Motors, etc). It was designed by a programmer who doesn't belong to the company I work. He is from a company from another country and he helps us remotly. I have to download the HMI project (a new one he sent us with some changes) to the HMI in the machine, but when I try to do it, it says that I should downgrade the device version: "a more recent incomptaible firmware exists on the target device". I try to fix it changing the version of the HMI, but the latest version I have available to select is v14.0.1, the project comes with v15.0 and I think the HMI is v15.1 so my question is: how can I update the versions available in the TIA Portal (v15.0 upd 4) to be able to choose 15.1? I attach a picture for easy understanding. [snip] |
Last edited by: DTCelectronicaAutomation at: 04/27/2020 05:38:27Last edited by: Jen_Moderator at: 04/27/2020 11:47:13Removed link and added file as an attachment. |
|
4/27/2020 2:44 AM | |
Joined: 7/5/2013 Last visit: 5/8/2024 Posts: 3083 Rating: (505) |
Hello DTC
to be able to choose 15.1, you have to install TIA V15.1. There you can use the same licenses as for TIA V15. You should check with your supplier if he recommends this and maybe he can even provide the updated software. Otherwise you can downgrade the panel from V15.1 to V15 by using ProSave which might be already installed with TIA (you find it on the installation-DVD resp. -file or download the latest version here (at the moment V16): Servicetool SIMATIC ProSave). Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to1 thankful Users |
4/29/2020 10:35 AM | |
Joined: 8/3/2009 Last visit: 5/10/2024 Posts: 12915 Rating: (1646)
|
Hello yes the upgrade and downgrade procedure ist a normal thing with HMI Panels like comfort Panels or Basic Panes. In TIA Portal you can choose theh Image Version from your current Version down to older Versions but you cannot use newer Versions like you have installed. You can check which FW Version the Panels has (Settings -> OP-> Device). In the Loading dialog you an activate the Up-/Downgrade and It should run automatically. If there are further Problems with the OS UPdate then you also can do a: https://support.industry.siemens.com/cs/ww/en/view/19701610 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on