6/3/2014 12:05 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Hello, I have not called SFC51 with a zero SZL-ID (SSL-ID) but I am sure it should return you an error via return value.List of possible SSL-ID can be found in section (34 System Status Lists (SSL)) of the following manual: http://support.automation.siemens.com/WW/view/en/44240604Even a real CPU may not respond to all SSL-IDs and also returns an error.So please check the feedback of the called block. Best regards, Hamid Hosseini |
This contribution was helpful to1 thankful Users |
6/5/2014 8:26 AM | |
Posts: 12 Rating: (0) |
Hi, I test SSL-ID = W#16#0000 on a real H-CPU(6ES7 417-5HT06-0AB0), it respons with 114 records. I check the record, it seems the SSL-ID support by that CPU. see attached file. AttachmentSSL_ID_0000.zip (237 Downloads) |
6/5/2014 10:24 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Hello again, I am sorry to say our data is bounded to documented values.For case related to "SSL-ID = W#16#0000" , a developer should answer.My suggestion would be contacting HERE. Good Luck ! Hamid Hosseini |
This contribution was helpful to1 thankful Users |
5/5/2020 2:58 AM | |
Joined: 1/1/2017 Last visit: 5/9/2024 Posts: 329 Rating: (11) |
Hi, Thanks a lot! Regards OmKris |
Follow us on