4/6/2022 9:05 AM | |
Joined: 5/10/2021 Last visit: 8/24/2022 Posts: 36 Rating: (1) |
I'm looking for this feature too, would be very helpful. |
9/16/2023 8:06 AM | |
Joined: 10/11/2020 Last visit: 2/10/2024 Posts: 36 Rating: (0) |
Did anyone ever find a solution to this issue? I have seen the AR app you can download that will display unified url and has guidance on how to setup. I've tried but can't get to a specific url / screen via the standard chrome or edge browser. https://cache.industry.siemens.com/dl/files/771/109820771/att_1141535/v1/UnifiedAR_V_1_0_en.pdf Generate a QR code for a web page with the QR code generator of your choice. Example URI of any HTML page: https://siemens.com https://siemens.com?w=600&h=600&text=Unified%20AR Example URI of a Unified Runtime with parameters: wincc://myhost.local?screen=ScreenName wincc://192.168.178.20?screen=ScreenXY&w=1920&h=1080 The following parameters are possible: “screen” (name of the screen to be displayed according to Engineering System) “w” width of the web page between 500 and 4096 “h” height of the web page between 500 and 4096 “text” Alternative display name instead of “screen” Special characters must be URL-encoded Print out the QR code or display it on a screen AttachmentUnifiedAR_V_1_0_en.pdf (299 Downloads) |
Last edited by: Jen_Moderator at: 09/25/2023 06:21:04PDF attached from link. |
|
9/22/2023 10:27 AM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641) |
Hello Terra70 As I know this is not supported/possible in a normal application without AR App. You can use QR Codes or other information on the Client to access diffferent screens but only if you use tags inside Unified or a CWC that can access local ressources like this one: https://support.industry.siemens.com/cs/ww/en/view/109792602 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on