5/18/2020 1:15 PM | |
Posts: 75 Rating: (0) |
Hello. I'm interesting again about sIEMENS Micromaster Integrated 6S 9612 7DF60ZC87 for pump DAB KLPE 65-1200T. Micromaster is not available any more so I need other compatible device for replacing. Which of theese is compatibility? MCE/C 11 – MCE/C 15 – MCE/C 22 MCE/C 30 – MCE/C 55 MCE/C 110 – MCE/C 150? Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/18/2020 13:54:42New subject after splitting |
|
6/2/2020 3:40 PM | |
Joined: 3/27/2008 Last visit: 9/12/2024 Posts: 1133 Rating: (142) |
The device which you have is 6SE9612-7DF(Y)0-Z=C87. Combimaster 1.1kW, 4.9 Ampere input current. A possible replacement could be: Motor, 1LE1001-0EB0, 90S frame 2.5 Amp. Power Module, 6SL3517-1BE13-3AM0, 1.1kW, 3.1 Amp output. Control Unit, 6SL3544-0MB02-1BA0, USS +Modbus RTU. In the above the Motor, Power unit, and control unit combine to create an inverter motor combination, qty 4 digital inputs, and qty 2 analogue inputs, qty 2 digital outputs. You must check with your local Siemens agent to confirm that the above components are suitable. The motor suggested here is a 90S, 4 pole device, but mounting needs to be confirmed. I hope this suggestion help with finding a replacement for the Combimaster. Tractor |
Tractor |
|
Follow us on