5/14/2020 5:23 PM | |
Joined: 1/24/2014 Last visit: 2/26/2024 Posts: 127 Rating: (6) |
Tia Portal V15.1 On this ScreenSaver, a big invisible button that call script 3 Another script 2 to randomise the position X and Y of the logo company max=879 min=0 SmartTags("SSx")= Int((max - min + 1) * Rnd + min) max=623 min=0 SmartTags("SSy")= Int((max - min + 1) * Rnd + min) <<<
Here my question :
|
5/18/2020 4:12 PM | |
Joined: 8/3/2009 Last visit: 4/23/2024 Posts: 12834 Rating: (1639)
|
Hello check out the Toolbox there are two simple examples for customized Screensavers: https://support.industry.siemens.com/cs/de/en/view/106226404 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on