5/13/2020 2:26 PM | |
Posts: 4 Rating: (0) |
Good Afternoon! I got a problem using the Arduino IDE with the IoT 2040 and was wondering, if someone could help me. Currently my PC does not detect the IoT 2040 when I plug it in. According to the Siemens Set up guide there should be a "Com Port" in my Devise Manager. How ever there is none. I also tried installing the Intel Driver manually, but that didnt work, too. I am currently on number 4.5 according to this (https://support.industry.siemens.com/tf/ww/en/posts/tutorial-program-the-iot2000-with-arduino-ide/164153/?page=0&pageSize=10 ) guide. One thing I noticed, is that the "USB"-Led is green all the time (even when there is no usb cable plugged in) Hope anyone can help me! Thanks in advance |
5/13/2020 3:59 PM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hey, are you using Windows10 or Windows7? Sometimes it is also needed to install the driver twice. This post is about this issue. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on