5/21/2020 2:48 PM | |
Joined: 6/29/2018 Last visit: 11/28/2023 Posts: 57 Rating: (2) |
Hello I have two kinds of SSR with analog input for power controlling, a 0-10 V and a 4-20 mA model. In this program by holding I1 and I2 the counter changes from 0 to 100. How to make an analog output from this counter? a 0-10v output and a 4-20mA output. AttachmentAnalog_Output_1.zip (174 Downloads) |
5/21/2020 3:10 PM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32886 Rating: (4066)
|
If you want to fully control the 0-10V output (or the 4-20mA output), you have to send 0-1000 units to the outputs. Therefore, the maximum value of the counter (100) must be multiplied by 10 after the counter. Attachment1399-03-01---Analog_Output_1_V2.zip (183 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on